Project Setup – Changed Parameters
Project Setup lets you quickly set up a variety of project information. The following parameters are organized according to the Project Setup page that lets you edit them.
System Definition screen
| 
                                                         Project Setup Setting  | 
                                                    
                                                         Section  | 
                                                    
                                                         Parameter Name  | 
                                                
|---|---|---|
| 
                                                         Resolution  | 
                                                    
                                                         MultiMonitors  | 
                                                    
                                                         Resolution  | 
                                                
| 
                                                         Style  | 
                                                    
                                                         MultiMonitors  | 
                                                    
                                                         IsHighContrast  | 
                                                
Servers
| 
                                                         Project Setup Setting  | 
                                                    
                                                         Section  | 
                                                    
                                                         Parameter Name  | 
                                                
|---|---|---|
| 
                                                         Advanced Reports Server  | 
                                                    
                                                         Applications  | 
                                                    
                                                         Hostname  | 
                                                
Menus in Project Setup
For each page selected in Project Setup (Step 5), the menu configuration items are added.
| 
                                                         Project Setup Setting  | 
                                                    
                                                         Section  | 
                                                    
                                                         Parameter Name  | 
                                                
|---|---|---|
| 
                                                         Monitor Count  | 
                                                    
                                                         MultiMonitors  | 
                                                    
                                                         Monitors  | 
                                                
| 
                                                         Monitor 1 Landing Page  | 
                                                    
                                                         MultiMonitors  | 
                                                    
                                                         StartupPage1  | 
                                                
| 
                                                         Monitor 2 Landing Page  | 
                                                    
                                                         MultiMonitors  | 
                                                    
                                                         StartupPage2  | 
                                                
| 
                                                         Monitor 3 Landing Page  | 
                                                    
                                                         MultiMonitors  | 
                                                    
                                                         StartupPage3  | 
                                                
| 
                                                         Monitor 4 Landing Page  | 
                                                    
                                                         MultiMonitors  | 
                                                    
                                                         StartupPage4  | 
                                                
| 
                                                         Monitor 5 Landing Page  | 
                                                    
                                                         MultiMonitors  | 
                                                    
                                                         StartupPage5  | 
                                                
| 
                                                         Monitor 6 Landing Page  | 
                                                    
                                                         MultiMonitors  | 
                                                    
                                                         StartupPage6  | 
                                                
| 
                                                         Monitor 7 Landing Page  | 
                                                    
                                                         MultiMonitors  | 
                                                    
                                                         StartupPage7  | 
                                                
| 
                                                         Monitor 8 Landing Page  | 
                                                    
                                                         MultiMonitors  | 
                                                    
                                                         StartupPage8  | 
                                                
In addition to parameters, you can do the following:
Servers, Network Addresses, and Computers
| 
                                                         Project Setup Location  | 
                                                    
                                                         Item  | 
                                                
|---|---|
| 
                                                         Step 3: Servers  | 
                                                    
                                                         Add I/O, Alarm, Trend, and Report Servers, primary and redundant 
 NOTE: Clusters are also added here.  | 
                                                
| 
                                                         Step 3: Servers  | 
                                                    
                                                         Add network addresses, primary and redundant  | 
                                                
| 
                                                         Step 5: Display: Menus and Display Pages  | 
                                                    
                                                         Create HMI menus: setup for graphics pages  | 
                                                
| 
                                                         Step 5: Display: Menus and Display Pages  | 
                                                    
                                                         Determine runtime landing pages at various monitors used in the project  | 
                                                
| 
                                                         Step 7: Device Profiles  | 
                                                    
                                                         Choose device profiles  | 
                                                
| 
                                                         Step 8: Devices  | 
                                                    
                                                         Add I/O devices; including equipment, ports, boards, I/O devices, variable tags, alarm tags, trend tags  | 
                                                
| 
                                                         Step 9: Finish  | 
                                                    
                                                         Compile and run the completed project  | 
                                                
Final - Compile and Run Project
When you select Compile and Run Project on the final screen, the following changes are made to the citect.ini file:
| 
                                                         Section  | 
                                                    
                                                         Parameter Name  | 
                                                    
                                                         Value  | 
                                                
|---|---|---|
| 
                                                         Lan  | 
                                                    
                                                         TCPIP  | 
                                                    
                                                         1  | 
                                                
| 
                                                         CTEDIT  | 
                                                    
                                                         Run  | 
                                                    
                                                         (Project's path)  | 
                                                
| 
                                                         CTEDIT  | 
                                                    
                                                         LASTDATABASE  | 
                                                    
                                                         (Project's name)  | 
                                                
| 
                                                         CTEDIT  | 
                                                    
                                                         LASTDATABASEPATH  | 
                                                    
                                                         (Project's path)  | 
                                                
| 
                                                         Client  | 
                                                    
                                                         ComputerRole  | 
                                                    
                                                         0  | 
                                                
| 
                                                         Client  | 
                                                    
                                                         FullLicense  | 
                                                    
                                                         0  | 
                                                
| 
                                                         Client  | 
                                                    
                                                         PartOfTrustedNetwork  | 
                                                    
                                                         1  | 
                                                
| 
                                                         Client  | 
                                                    
                                                         Clusters  | 
                                                    
                                                         (Comma separated list of available clusters for the project)  | 
                                                
| 
                                                         CtSetup  | 
                                                    
                                                         CustomSetup  | 
                                                    
                                                         0  | 
                                                
| 
                                                         Internet  | 
                                                    
                                                         Server  | 
                                                    
                                                         0  | 
                                                
| 
                                                         Alarm  | 
                                                    
                                                         SavePrimary  | 
                                                    
                                                         (Project's path)  | 
                                                
| 
                                                         Report  | 
                                                    
                                                         InhibitEvent  | 
                                                    
                                                         1  | 
                                                
| 
                                                         Report  | 
                                                    
                                                         RunStandby  | 
                                                    
                                                         1  | 
                                                
| 
                                                         Trend  | 
                                                    
                                                         InhibitEvent  | 
                                                    
                                                         1  | 
                                                
| 
                                                         Event  | 
                                                    
                                                         Server  | 
                                                    
                                                         0  | 
                                                
| 
                                                         Win  | 
                                                    
                                                         AltSpace  | 
                                                    
                                                         1  | 
                                                
| 
                                                         Server  | 
                                                    
                                                         AutoLoginMode  | 
                                                    
                                                         1  | 
                                                
| 
                                                         Server  | 
                                                    
                                                         EWSAllowAnonymousAccess  | 
                                                    
                                                         0  | 
                                                
| 
                                                         (ServerType.Cluster.ServerName)  | 
                                                    
                                                         StartupCode  | 
                                                    
                                                         PLS_StartAdvOneLine() *This is set on one IO server on each server machine in the project  | 
                                                
| 
                                                         (ServerType.Cluster.ServerName)  | 
                                                    
                                                         Clusters  | 
                                                    
                                                         (Comma separated list of available clusters for the project)  |