Managing device type categories
Use Set Up Device Type Categories to add, edit, and delete categories. These categories are used in the I/O Device Manager to logically group the list of profiles that display, and to make them easier to locate.
When you add device types in the Add/Edit Device Type screen, you associate a category and subcategory with each device.
To view the Set Up Device Type Categories screen, select Settings > Set Up Device Type Categories.
The following table describes the parts of this screen. Detailed instructions are after the table.
|
Field Name |
Valid Entries |
Comments |
|
Categories Options box |
Create New
|
Select to begin adding a new device type that is not based on an existing type. |
|
Edit Existing |
Select to begin editing the category or subcategory name. |
|
|
Delete Existing |
Select to begin deleting a category. You cannot delete a category that is associated with a device type. |
|
|
Category Name |
If new: Type the name. If editing or deleting, select the name from the drop-down menu. Predefined categories do not display. Currently, there is one predefined category: Schneider Electric. |
|
|
Subcategories Options box. |
As with categories, you can create new, edit existing, or delete. |
If new: Type the name. If editing or deleting, select the name from the drop-down menu. You cannot delete a subcategory that is associated with a device type. Predefined subcategories do not display. Currently, the predefined subcategories are: Protection Device, Monitoring Device, and PLC. |
Adding a category or subcategory
To add a category or subcategory:
- Select Create New in the appropriate box (Categories or Subcategories).
- In the Name field, type the name of the new category or subcategory.
- Select OK to save the new entry and close the screen.
Editing a category or subcategory name
To change the name of a category or subcategory:
- From the appropriate box, select Edit Existing.
- From the dropdown menu, select the category or subcategory that you want to edit.
- Type the new name for this category or subcategory.
- Select Save to make the change, or select Save & Exit to save changes and close the screen.
Deleting a category or subcategory
Predefined categories and subcategories, or those associated with a device type, do not display for deletion.
To delete a device type associated with a category or subcategory:
- Change to the Edit view
- Select the category or subcategory, then select List Device Types.
- Note the device types and go to the Add / Edit Device Types screen.
- Change the category or subcategory on that page.
- Return to the Set Up Device Type Categories screen to delete the category/subcategory.
To delete a category or subcategory:
- From the appropriate box, select Delete Existing.
- From the dropdown menu, select the category or subcategory that you want to delete.
- Select Delete.
- Select Yes to confirm the deletion.
- Select Save to save the change, or select Save & Exit to save changes and close the screen.