Building Operation Components and Snippets

The EBO integration files folder in PME ISO includes components and snippets for the creation of Graphics in Building Operation.

NOTE: These components and snippets were installed on the Building Operation server in a previous step. See 3. Installing the components, snippets, and binding template for details.

Components

Animated Components for ANSI and IEC

The EBO integration files folder in PME ISO includes a set of animated Components that are based on the American National Standards Institute (ANSI) and International Electrotechnical Commission (IEC) symbol standards. These can be used by the Building Operation Graphics Editor.

Static device images

The EBO integration files folder in PME ISO  includes a library of device images that can be used in the Building Operation Graphics Editor. Use the images represent the devices and equipment present in your system. They can be added to a diagram by selecting the device from the Meter Graphics category and dragging the image to the work area.

The library contains images for the following devices:

  • ION6200
  • PM5000 Series
  • ION7550/7650
  • EM3500 Series
  • PM700 Series
  • Acti 9 iEM 3000 Series
  • PM800 Series
  • Veris E50 Series
  • PM3200 Series

 

NOTE: Device images are available for: a). meters that are bound and show data, and b). meters that are not bound and show no data. Choose the device images that best represent your system.

Snippets

The EBO integration files folder in PME ISO includes a Building Operation snippet that is designed to be used with the ANSI and IEC components.

Advanced Tooltip Snippet

The Advanced Tooltip Snippet provides information regarding a specific device when the pointer hovers over it. The display text of the tool tip can be customized, and the following properties can be defined:

  • Font size
  • Font color
  • Number of decimal places to display
  • Measurements to show