Integration with EcoStruxure Building Operation - Configuring

Configuring the PME/EBO Integration solution includes the following steps:

  1. Configuring server settings
  2. Configuring communications
  3. Configuring PME Web Applications
  4. Integrating PME Web applications in Building Operation
  5. Setting up Graphics in Building Operation
  6. Configuring Dashboards and Slideshows

NOTE: These steps are required for both solution architectures, unless specifically called out in the workflow steps.

See the following sections for details.