Port Settings
PME
See IP Ports for more information.
Building Operation
The Enterprise Server uses HTTP and TCP protocols to communicate with other servers and clients. In the Software Administrator, you configure the port number of each protocol the Enterprise Server listens to when communicating through a specific protocol. Refer to the IT System Planning Guide - EcoStruxure Building Management for a full list of required open ports.
Changing Port Settings
Building Operation and PME both use the same HTTP (80) and HTTPS (443) ports by default. If you install Enterprise Server and PME on the same computer, you must change these ports for Building Operation to avoid a port conflict.
For example, use 8080 and 446 as shown below:
Therefore, during the design phase, the IT policy needs to be checked to make sure this is acceptable. If it is not, PME and the Enterprise Server should not be installed on the same computer and should instead be installed on separate servers.