Software compatibility
This section describes the PME/EBO Integration solution software compatibility as well as the operating environment requirements.
notice
LOSS of communication
| ● | Activate product and component licenses prior to the expiry of the trial license. |
| ● | Activate sufficient licenses for the servers and devices in your system. |
| ● | Export the existing hierarchy template out of Power Monitoring Expert before importing a new template. The new template can overwrite the existing template, which can permanently remove all information contained in the original. |
| ● | Backup or archive any SQL Server database data before adjusting any database memory options. |
| ● | Only personnel with advanced knowledge of SQL Server databases should make database parameter changes. |
Failure to follow these instructions can result in loss of data.
notice
UNAUTHORIZED OR UNINTENDED ACCESS TO CUSTOMER DATA
| ● | Personnel setting up the PME/EBO Integration third-party authentication must be aware that links to data are not secure. |
| ● | Do not setup access links to sensitive or secure data. |
Failure to follow these instructions can result in unauthorized or unintended access to sensitive or secure customer data.