5. Installing ETL (only for Architecture 1 solutions)
The ETL is only used with Architecture 1, where it copies historical data from Building Operation to PME. The ETL installer is included in the PME/EBO Integration Toolkit.
NOTE: On Windows Operating Systems with restricted permissions, the ETL tool might not initialize and load its plugins on start up. This is due to limited write permission on the ETL default install folder (...\Program Files\...). A possible solution is to install ETL to a custom folder with write permission (for example, C:\ETL).
To install the ETL
- In File Explorer, navigate to where you extracted the PME/EBO Integration Toolkit.
- Navigate to PME_EBO Integration Tools, and run the
ETL.exeto open the installer. - Follow the install pages and instructions, using the default settings where possible, until you have completed the installation.