Breaker Performance Module Design
The Breaker Performance Module monitors aging and wear of circuit breakers and reports on breaker protection settings. It provides historical and real-time information for aging and wear related breaker parameters. You can also set up alarming on these parameters.
Components
The following applications and features are used for this module:
- Breaker Aging Report
- Breaker Settings Report
- Vista diagrams
- VIP framework
- ION Software Modbus Gateway Service
- Breaker Aging Calculation Service
- Breaker Configuration Tool
Prerequisites
- This module can only be used with specific device types, see Supported devices for more information.
- The measurement data for the reports must be available as historical data logs in the database.
- This module requires a separate license. See Licensing for more information.
Design Considerations
- This module only works with the devices listed above under Prerequisites.
- Configuring this module takes time and expertise.
Related topics:
Breaker Performance Module topics
- Breaker Performance Module design
- Breaker Performance Module configuration
- Breaker Performance Module operation
Other software features
Other Software Modules