Computer Hardware
The performance of a computer is determined by the following factors:
- Computer type (desktop, workstation, or server)
- Central processing unit (CPU)
- Random-access memory (RAM)
- Data storage, for example Hard Disk Drive (HDD)
When choosing the computer hardware for your PME system, you need to consider the following:
- Number of devices in the system
- Number of concurrent users
- System performance expectations
- Data exchange with other systems
- Historical data logging needs
- System availability and recovery needs
NOTE: Undersized computer hardware is a common source of performance issues with PME systems.