Operating Environment
PME supports the following environments and software:
NOTE: The operating system and SQL Server combination you choose must be supported by Microsoft. This applies to edition, version, and 32-/64-bit.
NOTE: Apply the latest updates to the operating system and database system before installing or upgrading PME.
| Software | Supported Versions |
|---|---|
| Operating system |
Windows 10 Professional/Enterprise
|
| Database system** |
SQL Server 2014 Express |
| Virtual environment*** |
VMWare Workstation 10 |
| Microsoft Excel | Microsoft Excel 2013, 2016, 365 |
| Desktop Web browser |
Google Chrome version 100 and later
|
| Mobile Web browser |
Safari on iOS8.3+ operating systems, Chrome on Android systems |
| .NET Framework |
.NET 4.8 |
* For information on choosing an operating system, see Operating System considerations.
** PME includes a free version of SQL Server Express. You have the option to install this Express version during the installation of PME, if you don't want to use a different SQL Server.
*** You must configure virtual environments with a supported Windows operating system and SQL Server edition. It is possible to mix virtual and non-virtual environments for PME server and clients.