Planning checklist
The  following checklist has an entry for each of the sections in the planning chapter of this 
| Item | Details | Completed | 
|---|---|---|
| System Architecture | Decide which architecture to use (Standalone, Distributed Database). | □ | 
| Client Types | Decide which type of clients and how many of each are needed (Web Clients, Engineering Clients). | □ | 
| IT requirements | Decide which computer hardware, and operating software to use (OS, SQL Server). Understand the network related dependencies, and plan for them. | □ | 
| System maintenance | Understand the system maintenance needs and recommended actions. | □ | 
| Disaster recovery strategy | Understand on disaster recovery and recommended strategy | □ | 
| Licensing | Understand which licenses (PME, OS, SQL, ...) are required for your system and plan to purchase them in time for the deployment. | □ | 
| System installation and upgrades | Understand the prerequisites and the different options for new installs and upgrades. | □ | 
| Feature Selection and design | Define which features and modules you want to setup for the user. Understand the prerequisites and dependencies, and plan for them. | □ | 
| Device networks | Understand the device network options (Ethernet, serial). Match the devices with features and modules (device capabilities, performance, and so on). | □ | 
| Cybersecurity | Understand the security needs of your customer and application. Develop a security strategy and plan for the system, the network, the devices, and other relevant components (data encryption, virus and malware detection, firewalls, ...). | □ | 
| System integration | Understand the different approaches and technologies for integrating PME with other systems, for example, OPC, EWS, ETL, ODBC, PQDIF, VIP, .... | □ | 
| Deployment considerations | Understand the complexity of the deployment and the time and expertise required. | □ |