Before migrating the software
Review the prerequisites
Before starting the migration,
Backup the databases
Backup the ION_Data, ION_Network, ION_SystemLog, and ApplicationModules databases before starting the migration. Keep the backups in a secure and safe location. Use these backups to restore the original databases in case data is deleted or lost, accidentally, during the migration.
notice
LOSS of data
| ● | Back up the database at regular intervals. |
| ● | Back up the database before upgrading or migrating the system. |
| ● | Back up the database before trimming it. |
| ● | Back up the database before making manual database edits. |
| ● | Verify correct database behavior after making database or system changes. |
Failure to follow these instructions can result in permanent loss of data.
Cybersecurity
Review the cybersecurity information. See Cybersecurity for details.
Windows Integrated Authentication for SQL Server
If you are planning to install PME with Windows Integrated Authentication on the new system, see Windows Integrated Authentication for SQL Server for up-front configuration steps.
NOTE: Windows Integrated Authentication is not supported for PME systems with Secondary Servers.