System migration
Use a system migration to copy the configuration of one PME system to another PME system on a different computer. System migrations are performed manually with the Configuration Manager tool.
NOTE: System migration only applies to Standalone Serves and Application Servers. There is no migration for Engineering Clients.
Migrating a configuration from an old system to a new system using Configuration Manager is accomplished in six steps and must be done in the following order:
- Step 1 – Prepare both systems
- Step 2 - Transfer the Configuration
- Step 3 - Initialize the Configuration
- Step 4 - Manually Recreate Customizations
- Step 5 - Service the System
- Step 6 - Perform a Post-migration System Check
See Estimated task time for SBS upgrades for information on the expected upgrade time.
NOTE: The old PME system can keep running while the configuration is migrated. However, you might experience some performance degradation if two systems are working with the devices.