Requirements

To use the Configuration Manager, your Windows user account must have administrative rights on Windows and must exist as a Login in SQL Server with sysadmin role in the database instance.

Supported configurations

Configuration Manager 2023 supports configurations for systems with Standalone and Distributed Database architecture. It supports all language versions of PME. The following upgrade and migration paths are supported:

Source System Target System Architectures * Languages ** Editions ***
PME 7.2.2 PME 2023 All All All
PME 8.x PME 2023 All All All
PME 9.0 PME 2023 All All n/a
PME 2020 PME 2023 All All n/a
PME 2021 PME 2023 All All n/a
PME 2022 PME 2023 All All n/a
PME 2023 PME2023 All All n/a

* Architectures = Standalone and Distributed Database architectures
** Languages = The localized versions of PME
*** Editions = Standard Editions, Healthcare (HC) Edition, Data Center (DC) Edition, Buildings (BD) Edition

Limitations:

  • Changing languages between source and target system is not supported.
  • Archived configurations saved with an earlier version of Configuration Manager are not compatible with this release of the tool.

SQL Server Editions

If your archived configuration does not include historical data, you can migrate a system using any SQL Server edition combination. However, if your archived configuration includes historical data, migrate a system using the following:

Source SQL Server Edition Target SQL Server Edition
Express Express
Express Standard
Standard Standard

NOTE: You cannot restore data or configuration from a newer version of SQL to an older version. For example, if the source system uses SQL Server 2016, you cannot restore the configuration to a target system using SQL Server 2012.

Localization

The Configuration Manager is available in English only; it cannot be localized into other languages.