Reconfigure the System
The PME installer configures many settings when installing the software. During the configuration transfer using Configuration Manager, some of these settings are affected and must be reconfigured when Write to System completes.
Run the PME installer in Reconfigure mode on the target system after Write to System completes to ensure that all application settings are configured correctly.
NOTE: If manual changes to the Web Applications web.config file are required, then make those edits before reconfiguring the system. See Step 4 - Manually Recreate Customizations and Web Application web.config for more information.