Designer
Use Designer to configure nodes on your network that are based on ION Architecture. The node can be a software component or a hardware device.
NOTE: Only nodes based on ION Architecture can be configured using Designer.
Designer’s graphical user interface helps visualize a node's configuration. You can link ION modules together to customize a node for your particular application. You can also cut, copy and paste functionality within a single node or between different nodes.
                                                 warning
warning
unintended equipment operation
Do not use a controlled output for any safety critical application due to possible unexpected changes of state during power cycles, power outages, configuration changes, or firmware upgrades.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
Only personnel with a thorough understanding of ION architecture and the system in which the meters and software are installed can configure ION modules and registers.
For more information on ION Architecture, ION modules or ION registers, see the ION Reference.