Editing an OPC Device Type

You can use the Device Type Editor to modify existing OPC device types.

References

See the following references for information on how to use the Device Type Editor or information related to OPC tag definitions:

To edit an OPC device type:

  1. In Device Type Editor, click File > Open, find and select the device type you want to edit, and click Open.
  2. Modify the OPC tags or the Measurement Tree mappings to meet your needs.

    See Creating an OPC Device Type for details on how to perform these tasks.

  3. Click File > Save, to save the modified device type under the same name. Click File > Save As, to save the modified device type under a new name.
Related topics