OPC measurement support
OPC measurement support for Power Monitoring Expert allows you to easily translate data from 
Management Console has a command that lets you export default measurements from compatible devices to the OPC server. In addition, Designer and Device Type Editor user interfaces let you view and select which OPC measurement data you want the OPC server to expose to OPC clients.
Creating/updating default OPC mapping
Power Monitoring Expert can create the default ION-to-OPC data mapping based on the devices contained in the ION_Network database. This default mapping translates the most commonly-used 
- Launch Management Console.
 - Click Tools > System > Update OPC Server.
 - 
                                                
Click Yes to create/update the OPC server.
A summary of the configuration details is displayed.
 - Click OK.
 
NOTE: If you add a new device to the ION_Network database at a later date, you must repeat the above procedure in order to map the new source device’s data to the OPC server.