PQDIF Exporter main window

This is the main user interface for setting up schedules for PQDIF Exporter jobs or for setting up and running the jobs manually.

From Management Console, click Tools > System > PQDIF Exporter.

 
A Main menu items B Status of Exporter

Menu items

All the PQDIF Exporter commands are available from the main menu. Some of these commands are also available when you right-click on the interface background or on a job.

Starting/stopping the exporter service

To start the PQDIF Exporter service:

  • Select Options > Start Exporter Service, or
  • Right-click the status bar and select Start Service.

To stop the service:

  • Select Options > Stop Exporter Service, or
  • Right-click the status bar and select Stop Service.