Configure Generator Activity Report
warning
inaccurate data results
● | Do not incorrectly configure the software or the devices. |
● | Do not base your maintenance or service actions solely on messages and information displayed by the software. |
● | Do not rely solely on software messages and reports to determine if the system is functioning correctly or meeting all applicable standards and requirements. |
● | Consider the implications of unanticipated transmission delays or failures of communications links. |
Failure to follow these instructions can result in death, serious injury, equipment damage, or permanent loss of data.
To configure the Generator Activity Report:
- Set up the monitoring device that records the generator electrical data in PME. See Supported measurements and devices for details on which measurements are required.
- Create a Generator in the Generator Performance Configuration Tool with EPSS Test Module, and define, at a minimum, the following fields for this Generator:
- Name - Enter a name for the generator.
- Electrical Data - Select the Source of the electrical measurement data for the generator. Enter the generator Nameplate Rating and select the Unit.
- Status Measurements - Select the Source of the generator Status Measurements, and the measurements used to indicate the Running and Stopped states.
- Create a Transfer Switch in the Generator Performance Configuration Tool with EPSS Test Module, and define, at a minimum, the following fields for this transfer switch:
- Name - Enter a name for the transfer switch.
- Status Measurements - Select the Source of the transfer switch Status Measurements, and the measurements used to indicate the Normal, Test, and Emergency states.
NOTE: The transfer switch states are required for the Run Reason information in the report.
- (Optional) Repeat steps 2 and 3 to add additional generators and transfer switches.
- Create a Group in the Generator Performance Configuration Tool with EPSS Test Module, and define, at a minimum, the following fields for this Group:
- Name - Enter a name for the group.
- Generators - Select the Generators you created in step 2.
- Transfer Switches - Select the Transfer Switches you created in step 3.
- Open the report template in the Reports Web Application, set the report input parameters, and generate the report.
NOTE: The groups you create with the Generator Performance Configuration Tool are available for selection as inputs to the Generator Activity Report. All Generators that are defined in a group are included in the report when that group is selected. You have the option to exclude generators in a group from a report by selecting this option in the report inputs section.
For information on how to use the report, see Generator Activity Report.