Insulation Monitoring configuration (IEC)
To configure the Insulation Monitoring Module for facilities in the IEC market:
- Install and configure the devices and hardware components. See Insulation Monitoring Hardware Configuration for IEC for details
- Use the Insulation Monitoring Configuration Tool for IEC to:
- Configure the panels, areas, and groups.
- Generate Vista diagrams
- Set up the VIP framework and configure the Vista diagrams. See Configuring the VIP Framework and Vista Diagrams for IEC for details.
- Open the Insulation Monitoring report template in the Reports Web Application, set the report input parameters, and generate the report.
- View the diagrams in Vista or in Web Applications Diagrams.