Set up Power Quality Groups

The Power Quality Groups are defined per process (for example, a production line), so that only the power quality events captured by the meter which relate to the particular process are considered in the impact analysis.

Power Quality Groups must be defined or the Power Quality Impact gadgets and Report will not function.

The incomer meters defined in the Power Quality Groups are also used for the Power Factor section of the Power Quality Analysis Report.