Configure the Standardized Equipment Diagrams
The following sections describe how to set up and configure the Standardized Equipment Pages. Skip this section if corrective equipment does not exist in the system.
- Configure the Framework for the Equipment Diagrams
- Configure the Equipment Diagram Detail Pages
- Configure the Equipment Diagram Group Pages
- Configure the Equipment Diagram Landing Pages
Unlike the Power Quality Performance Indicator diagrams, the Equipment diagrams are not auto-functional pages, but rather templates that you use during commissioning to provide the user with equipment status displays with the same user experience and focus on simplification as the Power Quality Performance Indicator pages.
The equipment diagram elements are:
- Equipment Diagram Landing Pages
- Equipment Diagram Grouping Pages
- Equipment Diagram Detail Pages
Equipment Diagram Landing Pages
The Corrective Equipment Status portion of the Power Quality Performance page is a landing page.
The Equipment page is also a landing page.
Equipment Diagram Grouping Pages
When you select an element of the Equipment landing page (e.g. Capacitor Banks), the grouping page opens. A summary entry for each device (e.g. Capacitor Bank) in the system could be configured here.
Equipment Diagram Detail Pages
When you select an element on the Equipment Grouping Page, the equipment diagram detail page for that device opens.
The following supported devices currently have template pages available:
- Capacitor Banks: VarPlus Logic VL6 and VL12
- Active Harmonic Filters (AHF): Accusine PCS+/PFV+
- Uninterruptible Power Supplies (UPS): Galaxy 5000 and 5500
All Equipment Diagrams are installed in the following location:
{root install folder}\config\diagrams\ud\Equipment
Configuration Workflow
The order of commissioning is the opposite of user workflow. Set up the Detail Pages first, and then create the buttons for each Detail Page on the Group Pages. The Landing Pages (both Equipment and PQ Performance Indicator), require no commissioning other than optional customization if required.