Open the Power Quality Indicator Diagrams

The PQ Indicator Diagrams are located in:

{root install folder}\config\diagrams\ud\PQPerformance

The diagrams start to function once the framework is pasted in the Power Quality Performance VIP. You can link them to the existing Vista diagrams or use them separately.

NOTE: When a Power Quality Indicator has no supported device to feed it the required data, it should be disabled by following the procedures in the section Disable unused Power Quality Indicators.

Alternative symbols can be used to provide a colorblind friendly view. They are located in the folder:

{root install folder}\config\diagrams\images\PQPerformance\Indicators\Alternate\

Set the Query Server – Distributed system only

When using distributed PME systems, set the query server node for the following landing page diagrams:

  • LandingPage_24h.dgm
  • LandingPage_7d.dgm
  • LandingPage_30d.dgm
  • LandingPage_12m.dgm