Enabling time synchronization
Time synchronization is crucial for:
- Event clustering (the same event seen by different devices is only counted once).
- Correctly associating the process impact alarms with power quality events.
The standard synchronization between the Power Monitoring Expert server and devices is adequate for enabling Power Quality Performance features.
- For Modbus devices, time synchronization through Modbus is activated by default.
- For all ION protocol devices (e.g. ION7650, PM8000, etc.), the application engineer needs to enable this feature.
NOTE: High accuracy of time synchronization (such as IRIG-B, etc.), can be used to address user requirements, but it is not required for Power Quality Performance.
To enable Power Monitoring Expert time synchronization on an ION device:
- Connect to the device using ION Setup. On the Timezone tab for Clock, change entry for the CL1 Time Sync Source to ETHERNET - ION. You can also do this on the meter front panel.

- In Management Console:
- For an Ethernet device, set the Time Synch Ethernet Enabled to Yes in the Ethernet Device Configuration.

- For a serial device, set the Time Synch ION Enabled to Yes in the Ethernet Gateway Site Configuration.

- For an Ethernet device, set the Time Synch Ethernet Enabled to Yes in the Ethernet Device Configuration.