Configuring switchboards
To configure switchboards:
- In the Breaker Configuration Tool, click the Switchboards tab, and then click New to add a new Switchboard.
- Enter the following information:
- Name: Enter a unique name for the switchboard.
- Breakers: Select one or more breakers from the list. Each breaker can only be associated with one switchboard in the system.
- Enter the following information:
- Critical Threshold % and Moderate Threshold %: Enter default values (0-100%) to be used for each breaker associated with this switchboard when performing analysis of their electrical aging and electrical wear levels.
- Environmental Conditions: Select values for Switchboard IP, Salty Atmosphere, Corrosive Gas, and Dust Level.
- Current Environmental Data: Select values for Vibration Level, Humidity, and Temperature.
- (Only for Breaker Aging) Select Apply Historical Data if the switchboard is pre-existing in your electrical system. Clear the check box for Apply Historical Data if this is a new switchboard in your electrical system. For pre-existing switchboards, select values for Vibration Level, Temperature, and Humidity.
- Click Apply to save the changes and keep the configuration tool open. Click OK to save the changes and close the configuration tool.
-
(Optional) Repeat steps 1-5 to add additional switchboard devices.