Assigning engine data

The Assign Engine Data Measurements editor is used to map PME engine measurements to engine data that is recorded by a monitoring device for the generator engine.

To assign engine data:

  1. Click Assign Engine Data to open the Assign Engine Data Measurement editor.
  2. Click New to add a new assignment. Complete the following fields:
    • Engine Data Measurement - Select the measurement you want to assign.
    • Source - Select the monitoring device that records the engine data of the generator.
    • Measurement - Select the monitoring device data that you want to map to the engine measurement.
  3. (Optional) Repeat step 2 to map additional measurements.
  4. Click OK to save the measurement mapping and close the Edit Engine Data Measurements window.

TIP: See Editing Engine Data for information on how to define engine measurements.