Cloning a Generator

Clone a Generator to create a copy of an existing Generator. When you clone a Generator, many of the settings are copied into the new Generator. Some settings are reset to default values. Update the settings for the cloned Generator and save it.

To clone a Generator:

  1. On the Generators tab, select the Generator you want to use as the base for the cloned copy.
  2. Click Clone to create a new, cloned Generator. Review the copied settings and update them as necessary. Update the following settings that have been reset to default values:
    • Name - Enter a unique name to identify the Generator.
    • Electrical Data - Source - Select the monitoring device that records the electrical data of the generator.
    • Status Measurements - Source - Select the monitoring device that records the generator states.

    See Adding a new generator for information on generator properties.

  3. Click Apply to save the changes and keep the configuration tool open. Click OK to save the changes and close the configuration tool.