Cloning a Transfer Switch

Clone a Transfer Switch to create a copy of an existing Transfer Switch. When you clone a Transfer Switch, many of the settings are copied into the new Transfer Switch. Some settings are reset to default values. Update the settings for the cloned Transfer Switch and save it.

To clone a Transfer Switch:

  1. On the Transfer Switches tab, select the Transfer Switch you want to use as the base for the cloned copy.
  2. Click Clone to create a new, cloned Transfer Switch. Review the copied settings and update them as necessary. Update the following settings that have been reset to default values:
    • Name - Enter a unique name to identify the transfer switch.
    • Status Measurements - Source - Select the monitoring device that records the transfer switch states.

    See Adding a new Transfer Switch for information on transfer switch properties.

  3. Click Apply to save the changes and keep the configuration tool open. Click OK to save the changes and close the configuration tool.