Adding/Editing Group Load Sources

Define Load Sources to associate a Group with the electrical loads that the generators in the group must supply with power during an outage.

NOTE: Before configuring Load Sources, define the Priority Levels for the system. See Editing Transfer Switch priority levels for details.

To add/edit group load sources:

  1. Click Edit Load Sources to open the load sources editor.
  2. In Edit Load Sources, click New to add a load source.
  3. Complete the following fields:
    • Source - Select the monitoring device that records the electrical data of the load.
    • Measurement - Select the load measurement.
    • Priority Level - Select the priority level to assign to the load.
  4. Click OK to save the configuration and close the Edit Load Sources window.

    TIP: Use Clone to define additional loads with similar settings.