EPSS Vista Diagrams
EPSS Vista diagrams provide real-time information about the status of the generators, transfer switches, and other components of the system. You can view the diagrams in the Diagrams Web Application of PME.
After the Generators, Transfer Switches, and Groups are configured, you can generate the Vista diagrams for the configured devices. The same information can be built manually in Vista, but the Generator Performance Configuration Tool with EPSS Test Module provides a way to build these diagrams automatically.
See Setting up the EPSS template diagram and Generating the EPSS Vista diagrams for instructions.
After the diagrams are generated, you can open them in Vista and optimize the designs. See EPSS Vista diagram examples for descriptions and examples of the generated diagrams.