Generator Power configuration restrictions
The Generator Power configuration tool enforces certain rules when creating a generator system, group, or generator:
- Generator System
- Name must be unique.
- One or more systems are allowed.
- Generator Groups
- Name must be unique.
- At least one group must be present in each system.
- All groups are connected to the same load.
- For N, N+1, and N+2 system types:
- Only one group is allowed.
- Each generator in the group must have the same nameplate rating (kVA) value.
- Each generator in the group must have the same derated nameplate rating (kW) value.
- For 2N, 2(N+1) and 2(N+2) system types:
- Up to three groups are allowed.
- All groups must have the same number of generators.
- All generators in the groups must have the same nameplate rating (kVA) value.
- All generators in the groups must have the same derated nameplate rating (kW) value.
- Generators
- Name must be unique.
- At least one generator must be present in each group.
- A maximum of 12 generators is allowed in each group.
For information on generator redundancy types, see Generator system redundancy types.