Defining Isolated Power Panels (ANSI)

Associate Line Isolation Monitoring devices (LIM-IG6) and Fault Location monitors (Bender EDS) with power panels.

To add a new Isolated Power Panel:

  1. Click the Panels tab and then click New.
  2. Enter the following information:
    • Device: Select a Line Isolation Monitor device for this panel.
    • Display Name: Enter a name for the device.
    • Fault Location Devices: (Optional) Select the fault location monitoring devices that are connected to the Line Insulation Monitor.
    • Monitoring Options: (Optional) Select the monitoring options that are configured for the Line Isolation Monitor device.

    NOTE: All Fault Location monitoring devices, Bender EDS, that are configured in the system are displayed automatically in the Fault Location Devices list. If no devices are displayed, that means that none are configured in the system.

  3. (Optional) Repeat steps 1 - 2 to add additional Isolated Power Panels.
  4. Click Apply to save the changes and keep the configuration tool open. Click OK to save the changes and close the configuration tool.

To update an existing Isolated Power Panel:

  1. On the Panels tab, click the Isolated Power Panel you want to update.
  2. Change the name, panel, and monitoring device selections as needed.
  3. Click Apply to save the changes and keep the configuration tool open. Click OK to save the changes and close the configuration tool.

To delete an existing Isolated Power Panel:

  1. On the Panels tab, click the Isolated Power Panel you want to delete.
  2. Click Delete.

NOTE: Regenerate the Vista diagrams after changing the Isolated Power Panel configuration.