Defining Isolated Power Panels (IEC)
Associate Insulation Monitoring (IM) devices and Insulation Fault Locator (IFL) devices with power panels.
To add a new Isolated Power Panel:
- Click the Panels tab and then click New.
- Enter the following information:
- Device: Select the IM device for this panel.
- Display Name: Enter a name for the device.
- Fault Location Devices: (Optional) Select the IFL device for this power panel.
- (Optional) Repeat steps 1 - 2 to add additional Isolated Power Panels.
- Click Apply to save the changes and keep the configuration tool open. Click OK to save the changes and close the configuration tool.
NOTE: All IFL devices that are configured in the system are displayed automatically in the Fault Location Devices list. If no devices are displayed, that means that none are configured in the system.
To update an existing Isolated Power Panel:
- On the Panels tab, click the Isolated Power Panel you want to update.
- Make the changes as needed.
- Click Apply to save the changes and keep the configuration tool open. Click OK to save the changes and close the configuration tool.
To delete an existing Isolated Power Panel:
- On the Panels tab, click the Isolated Power Panel you want to delete.
- Click Delete.
NOTE: Regenerate the Vista diagrams after changing the Isolated Power Panel configuration.