Defining UPS modules for Power Losses
To define a UPS module used in your power losses system:
- Click the UPS Modules tab.
- Click New. The editable fields are enabled.
- Define the UPS module:
- Name: Enter a unique name for the UPS module.
- Description: (Optional) Enter a description for the UPS module. For example: make, model.
- Input Side Meter Source: Select a source name from the drop-down list. The source represents the Power Monitoring Expert device that records the electrical data from the input side of the UPS module.
- Output Side Meter Source: Select a source name from the drop-down list. The source represents the Power Monitoring Expert device that records the electrical data from the output side of the UPS module.
- Click OK to save the UPS module.
Related Topic: Defining transformers for Power Losses