UPS Configuration Tool
TIP: You can open the UPS Configuration Tool from the Power Monitoring Expert > Configuration Tools folder on your desktop.
Use the UPS Configuration Tool to configure the Backup Power Module. With this tool you create UPS Devices and Groups for the UPS Auto Test Report, and you generate UPS Auto Test Vista diagrams.
 
Prerequisites
- The UPS devices must be configured in the PME Management Console and must be communicating before you can configure the components and properties in the configuration tool.