Defining UPS loads
A UPS load represents the logical load attached to a UPS group. This logical load has no functional purpose in the calculations for power redundancy. The UPS load is used only to provide a more complete diagram representation for the UPS system.
To define a UPS load:
- Click the UPS load element in the system diagram. The Properties screen appears.

- Complete the details for the UPS load:
- Load Name: Enter a name for the load.
- Description: Enter a description for the load. This field is optional.
- Click Done to save the UPS load.
Related Topics: