Enabling or disabling a processed measurement

Disable a processed measurement to remove it from the measurement list. Enable a processed measurement that was previously disabled to remove from the measurement list.

To disable a processed measurement using the Device Replacement user interface:

  1. In Device Replacement, select the Processed Measurement tab.
  2. Select the row of the processed measurement you want to edit and then click Disable in this row.

    NOTE: On disabled processed measurement, Click View to see the device and measurement selection.

To enable a processed measurement using the Device Replacement user interface:

  1. In Device Replacement, select the Processed Measurement tab.
  2. Select the row of the processed measurement you want to edit and then click Enable in this row.

 

Related topics:

For reference information see Device Replacement user interface