Re-configuring EWS Client
Re-configure an EWS client to update the EWS client configuration or the mapping information. You can edit one EWS client at a time using the EWS Client user interface.
warning
potential compromise of System availability, integrity, and confidentiality
Use cybersecurity best practices when configuring user access.
Failure to follow these instructions can result in death, serious injury, equipment damage, or permanent loss of data.
Cybersecurity policies that govern user accounts and access – such as least privilege and separation of duties – vary from site to site. Work with the facility IT System Administrator to ensure that user access adheres to the site-specific cyber security policies.
To edit an EWS Client using the EWS Client user interface:
- In EWS Client table, select the row of the EWS client for which you want to edit, and then click Edit
in this row. This opens the Re-configure EWS Client dialog.
- In Re-configure EWS Client, select the Configuration tab.
- In Configuration, update the configuration settings as needed.
- In Re-configure EWS Client, select the Device and Measurement Mapping tab.
- In Device and Measurement Mapping, update the mapping settings as needed.
- Click OK.
Related topics:
- Configuring EWS Client
- Re-configuring EWS Client
- Deleting an EWS Client
- Disabling or Enabling an EWS Client
For specific information on mapping, see
- Remapping a Device, Measurement, and / or Alarm Mapping
- Deleting a Device, Measurement, and / or Alarm Mapping
- Enabling or Disabling a Device, Measurement, and / or Alarm Mapping
For reference information see: