Creating a one-line on a graphics page

Build a one-line by adding components to the new page. Each component has properties and conditions that control the display.

To begin creating a one-line:

  1. In the Power Monitoring Expert folder, open the Graphics Editor.
  2. From the left pane, drag and drop a component in the Design workspace.
  3. Set the various properties to animate the one-line diagram. These properties include such information as BaseColor and StrokeWidth.
    1. All components must have a background rectangle with an opacity of .01
  4. Each component type requires specific properties and conditions to be set.

Before you can view your one-line, you must edit the menu structure, which controls the appearance of the graphics page. For more information, see Defining the Diagrams menu structure.

For information on how to configure graphics on a one-line, see the following topics: