Alarm Views
Use the alarm view settings to:
- Change the number of items that are displayed in the alarms display.
- Change the priority classifications for alarms and incidents.
- Customize the behavior of the alarm annunciator with these settings.
- Customize the display of Load Impact events in Alarm and Incident views.
To change how many Incidents, Alarms, and Events are shown in the Alarm Viewer:
- Under Display Settings, enter the maximum number you want to be displayed for Incidents, Alarms, and Events in the boxes.
- Click Save to apply the changed settings.
To change the Alarm Viewer update interval:
- Under Display Settings, select the Update Interval.
- Click Save to apply the changed settings.
To turn the Alarm Annunciator on or off:
- Under Annunciator, turn Enable on or off.
When the Annunciator is turned off, it is not visible in the Web Applications banner.
- Click Save to apply the changed settings.
To change what type of state counts are shown in the Alarm Annunciator:
- Under Annunciator, select the state type for Show counts for.
- Click Save to apply the changed settings.
To change the Alarm priorities that are shown in the Alarm Annunciator:
- Under Priority Classification, select or clear the Visible in Annunciator check boxes for the Alarm priorities you want to include or exclude from the Annunciator.
- Click Save to apply the changed settings.
To change for which Alarm priorities an Alarm notification sound is played:
- Under Priority Classification, select or clear the Audible in Annunciator check boxes for the Alarm priorities you want a notification sound to be played for or not.
- Click Save to apply the changed settings.
To change the sound that is played for Alarm notification:
- Under Annunciator, click Select Sound File.
- In Select Audio File, select the sound you want, or if the sound is not in the Media Library,
- Click Upload Audio File and either choose a sound file available on your system by clicking Choose Files or drag a sound file into the application area.
- Click Finish to add it to the Media Library.
- Click OK to complete your sound selection.
- Click Save to apply the changed settings.
To change the Alarm Annunciator update interval:
- Under Annunciator, select the Update Interval.
- Click Save to apply the changed settings.
To change the display color and Alarm priority ranges for the Alarm Viewer:
- Under Priority Classification, set the Color and Start values for the different alarm priorities. The End values are adjusted automatically.
- Click Save to apply the changed settings.
To change the display of Load Impact events in Alarm and Incident views:
- Under Load Impact Display, select or clear the check boxes for the options you want or not.
- Click Save to apply the changed settings.