Report Theme

Change the Report theme to customize the Reports colors and the Reports logo.

To change the Reports colors:

  1. Under Report Colors, select Use Theme Colors or Override Theme Colors.

    TIP: The system theme colors are defined by the System Theme settings for the Web Applications. See System Theme for more information.

  2. If you choose Override Theme Colors, then set the colors for the Report Title, Section Header, Table Header, Summary, Row Shading, and Section Title, using the drop-down selectors.
  3. Click Save to apply the changed settings.

To change the Reports Logo:

  1. In SETTINGS, open the Settings Library and click Report Theme.
  2. Under Report Logo, click Select to open the Select Report Logo Image dialog.
  3. Select an image currently available in the repository, or
    1. Click Upload Image to choose an image file available on your system or drag an image file into the application area.
    2. Click Finish to add it to the image repository.
  4. Click OK to complete your selection.
  5. Click Save to apply the changed settings.

NOTE: You can use GIF, JPG, JPEG, or PNG image formats. The recommended file size is 250 x 100 pixels. Images are automatically re-sized to fit the logo area in Reports.