Session Timeout

Use the session timeout settings to define the timeout behavior of the software web applications and Windows applications clients.

You have to following options:

  • You can enable and set a timeout for the web applications.
  • You can enable and set a timeout for the Windows applications.

NOTE: You can enter a timeout value from 1 minute to 1440 minutes (1 day)

When a session timeout is configured, web application clients are logged out and Windows application clients (Vista, Designer, Management Console) are locked after a period of inactivity. The default timeout for both client types is 20 minutes. To restart or unlock the session you must enter the login credentials.

A session is considered inactive when none of the following actions are detected for the duration of the timeout period:

  • Mouse movement
  • Mouse clicks
  • Keyboard activity
  • Touch screen activity