Duplicating an Alarm Rule
Duplicate an existing Alarm Rule to save time when creating a new Rule that is similar to an existing Rule.
To duplicate an Alarm Rule:
- In Software Alarms, select the Alarm Rules tab.
- In the Alarm Rules table, find the row of the Rule which you want to duplicate, and then click Duplicate
in this row to open the Edit Alarm Rule window.
TIP: You can also duplicate an Alarm Rule through the Duplicate command in the right-click context menu.
- In Edit Alarm Rule, review the Rule settings in the different tabs and update the settings for the duplicated Rule as needed.
- Click Save.
Related topics:
- Adding a new Alarm Rule
- Enabling or disabling an Alarm Rule
- Editing an Alarm Rule
- Duplicating an Alarm Rule
- Deleting an Alarm Rule
- Using the Setpoint Calculator
- Adding a Schedule
- Software Alarms configuration
For reference information see: