Database Manager
Use Database Manager to manually perform operations on the Power Monitoring Expert databases.
notice
LOSS of data
| ● | Back up the database at regular intervals. | 
| ● | Back up the database before upgrading or migrating the system. | 
| ● | Back up the database before trimming it. | 
| ● | Back up the database before making manual database edits. | 
| ● | Verify correct database behavior after making database or system changes. | 
Failure to follow these instructions can result in permanent loss of data.
NOTE: Database Manager does not include manual database  operations on the Application Modules database (ApplicationModules). In a disaster recovery situation or when directed by Technical Support, the Application Modules database can be restored by using the Restore database function in the SQL Server Management Studio. See Restoring a database for further information about this operation. 
For information on database maintenance tasks in PME, see Database maintenance.