Billing Reports
NOTE: These reports are part of the Energy Billing Module. This module requires a separate license.
PME includes the following billing report templates:
- Billing Report
- Billing Summary Report
- Billing Verification Report
- Multiple Billing Export Report
- Multiple Billing Report
CAUTION
inaccurate data results
| ● | Do not incorrectly configure the software or the devices. |
| ● | Do not base your maintenance or service actions solely on messages and information displayed by the software. |
| ● | Do not rely solely on software messages and reports to determine if the system is functioning correctly or meeting all applicable standards and requirements. |
Failure to follow these instructions can result in injury or equipment damage.
For information about changing the unit cost values in a rate file used for billing reports, see the Rate Editor tool.