Dashboard - Portrait Report
Summary
The Dashboard - Portrait Report shows screen captures of a dashboard slideshow in a portrait page layout. Use this report to share dashboard and Web content in any of the supported report formats, such as PDF and so on.
Details
You can include the screen capture of an additional, custom page by specifying the page URL.
TIP: Create separate slideshows for each dashboard page you want to report on.
Prerequisites
- A Dashboard slideshow must be configured.
Report inputs

Type a title for the report in the text box.

Select from the dropdown list. Select Fit to Page to automatically scale each output page to fit onto a single report page. Select Custom to scale the output based on the height and width values provided in the Custom Page Height and Custom Page Width boxes.

Specify a custom output page height. This value is ignored if Page Size is set to Fit to Page.

Specify a custom output page width. This value is ignored if Page Size is set to Fit to Page.

This box shows all available slideshows in your system. Select the slideshows you want to include in the report.

(Optional) Specify the URL for any page or image that you would like to include in the report. This could be a page from an external or internal website, or a local image.

Specify the maximum time the report waits for the slideshow or custom URL to load. If you selected multiple slideshows, then this maximum wait time is applied to each of the slideshows. If a slideshow or URL loads faster than the maximum wait time, the report completes before this time has elapsed.

Click Yes to include the standard report header and footer in the report. Click No to not include the standard report header and footer in the report.
The standard report header includes the logo, report title, and report generation information.

Click Yes to include data warnings in the report. If there are none, the section is not included. Click No to exclude this section.