Harmonic Compliance Report - Legacy
Summary
The Harmonic Compliance Report shows an analysis of the harmonic compliance of selected sources based on the IEEE 519-1992 standard. Use this report for an analysis and compliance assessment of your facility against the IEEE 519-1992 harmonics standard.
NOTE: This report needs data from monitoring devices with IEEE 519-1992 monitoring capabilities.
Prerequisites
- The measurement data must be available as historical data logs in the database.
Report inputs

Type a title for the report in the text box.

Use this input to select the devices you want to include in the report.
Click Select Sources to open the Source Selector dialog. From the Grouping list, select the way in which you want to display the sources (for example by device type, by group name, and so on). Click + and - to expand and collapse items in the navigation tree. Click the check box beside a device (or group of devices) to select it. Click Select All or Select None in the top-right corner to select or clear all the check boxes.
After selecting the devices, click OK.

Use this input to select the timeframe for the data you want to view in the report.
Select the reporting period from the dropdown list. The timeframe options in the timeframe dropdown are relative to the date the report is run. To run a report that starts and ends in the past, select the fixed date option. Type a start and end date in the date boxes or click the arrows beside the dates to display a pop-up calendar and select a date. Type a time in the time boxes or click the up and down arrows beside the time to adjust the hours or minutes up or down. You can also run a report that starts and ends in the future. You must manually add the future data. You can use any tool to generate future data. For example, use Manual Data Editor to manually enter measurement data.
Select the timezone you want to view timestamps in.

Use this field to add comments that will appear at the bottom of the generated report.

Select whether or not to include charts showing the total harmonic distortion (THD) of the voltage waveform, and the total demand distortion (TDD) of the current waveform, in the generated report. The default is Yes.

Select whether or not to include charts showing the average values related to harmonic compliance. The default is Yes.

Select whether or not to include charts showing a second level of harmonic compliance detail for the generated report. The default is No.

Select whether or not to force the y-axis to start at zero rather than scaling the chart normally. The default is Yes.

Click Yes to include data warnings in the report. If there are none, the section is not included. Click No to exclude this section.
Example:
NOTE: This example only shows selected content from the report, it does not show the entire report.