Default maintenance task settings
The default PME database maintenance tasks are defined as Windows PowerShell scripts, and scheduled and executed using Task Scheduler in Windows. The following table shows the different configuration settings for these tasks, their defaults, and where they are configured:
| Setting | Location | Default Value | Comments |
|---|---|---|---|
|
Windows account used to run the task |
Task Scheduler |
User account that is creating the task. |
Use IONMaintenance for Standalone systems. |
|
Task trigger times |
Task Scheduler |
The default schedules are configured automatically for Standalone systems. |
|
|
Task enabling or disabling |
Task Scheduler |
n/a |
|
|
Backup folder location |
PowerShell script : Configuration.ps1 |
...\ |
Sets the folder to which the database backups are saved. The backup script will create the following subfolders in this location: ...\Data for ION_Data |
|
Archive folder location |
PowerShell script : Configuration.ps1 |
...\ |
Sets the folder to which the database archives are saved. |
|
Data to keep when trimming |
PowerShell script : Configuration.ps1 |
30 |
Sets how many days' worth of data is left in the database after trimming. |
|
Database size (max)** |
PowerShell script : Configuration.ps1 |
9 |
Sets the maximum database size. This value is used by the size notification task to assess what percentage of database space has been used. The maximum size for a SQL Express database is 10GB. The maximum size in the script is set to 9GB to allow for a 1GB warning buffer before the database stops logging data. |
|
Database size notification limit** |
PowerShell script : Configuration.ps1 |
85 |
Sets the threshold for when a database size notification will be issued. |
* Default setting for Standalone systems.
** The database size notification is only configured for systems with SQL Server Express databases.