Extract task: Setting parameters and recommended values
Extract task settings
|
Setting Name |
Description |
Setting Parameters / Recommended Values |
|---|---|---|
|
Web Service |
||
|
Number of threads to use |
The maximum number of threads to use when contacting the EWS server for the list of Trend logs. Set value to 4 for most cases, however, set value to a lower number if the EWS server is overwhelmed with requests. |
Enter a value of 4. |
|
Timeout (in minutes) for EWS response |
The length of time (in minutes) to wait for a response from the EWS server when requesting information. |
Enter a value of 10. |
|
Web Service User Name |
The user name for Web Service. |
Provide EBO Workstation user name. |
|
Web Service Password |
Password for the Web Service user name. |
Provide EBO Workstation password. |
|
Web Service URL |
The URL of the EcoStruxure Web Service called by this task. |
Provide URL information. Default URL http://localhost:8080/EcoStruxure/DataExchange. NOTE: For HTTPS EcoStruxure Web Service connections, with a self-signed certificate, the certificate validation must be disabled for ETL. |
|
Communication Options |
||
|
Enable the Digest Authentication Token Reuse Feature |
When set to True, ETL will reuse digest authentication tokens for communicating with the EWS server. This can improve communication performance. |
Set to 'True' |
|
Reading Interval |
||
|
Interval Length Discovery |
When set to True, allows the extract task to determine the reading interval for each pair based on each pair's data. |
Set to 'True' |
|
Record State Filter |
|
|
|
Limit Results Based on Record State |
When set to True, enables a check on record state. Only records with a specified record state will be used. all other records will be ignored. When set to false, check is disabled and all records regardless of their record state are used. |
Set to 'False' |
|
Allowed Record State |
Sets the specific record check to be used by the Limit Results Based on Record state setting. Record states can be Good, Uncertain, Forced, Offline, or Error. |
Value not used if Limit Results setting is 'False'. |